Home /

Press Releases for Europe 


 
Provide feedback



Press Releases for Europe
About Renesas
Press Contacts


Notices


Seminars and Events





Press Release. Ref:REN0132(A1)

Renesas Technology announces compact, high-performance digital amplifier that supports IIS digital audio signal input


Click to View

LONDON, UK – 27th November 2008 - Renesas Technology Europe today announced the R2J15116FP, a compact, high-performance digital amplifier supporting IIS*1 digital audio signal input with a built-in 24-bit audio DSP. It is intended for use in thin flat-screen TVs employing LCD or plasma display panels.

The device, contained in a compact 7 mm x 7 mm package, accepts IIS digital audio signal input, performs signal processing using a built-in 24-bit audio DSP, and amplifies the result with a digital amplifier to deliver stereo output to two speakers at up to 15 watts per channel. Typically, thin flat-screen TVs require detailed tuning of their audio systems for different markets and screen sizes. This processing is usually performed in the preceding stage of this digital amplifier by the main DSP, which mainly handles tasks such as surround processing and decoding. This imposes a significant processing load. In the R2J15116FP, in contrast, processing for the volume control and the parametric equalizer*2 for optimizing the speaker characteristics is done by the built-in audio DSP. This reduces the load on the main DSP and makes it possible to generate a more varied and higher quality sound environment for video applications.

The R2J15116FP also achieves better audio signal performance and quality than conventional digital volume control implemented using a DSP, through the use of Renesas Technology’s exclusive intelligent volume function, which offers higher resolution when switching the volume level for smoother volume level transitions. The R2J15116FP also uses a feedback circuit to stabilize the output level when the power supply voltage fluctuates, an approach with a proven track record in products employing analog input. In addition to the volume control and seven-band parametric equalizer, there is a two-band tone control, a loudness function useful for low- and high-range expansion compensation, a power limiter function that allows setting of a user-defined maximum output level, and a dynamic range control (DRC) function that lowers the signal amplitude without distortion at high volume levels and raises it at low volume levels. Settings for all of these functions can be made flexibly from the MCU via the I2C bus.

Protection functions include detection of overcurrent, overheating, and low voltage, as well as a feature that provides warning in advance of overheating. This automatically lowers the volume to prevent the temperature from rising to a dangerous level. Additional functions include PLL unlock detection, which enhances the safety of signal input to the amplifier, and input signal error detection. This full complement of protection functions simplifies system design and boosts reliability.
The R2J15116FP uses a compact 48-pin HTQFP package, requires no heat sink, and delivers maximum stereo output of 15 watts per channel.

< Notes >
1. IIS: A widely used output format for digital audio signals.
2. Parametric equalizer: The equalizer in an audio processing system allows raising or lowering of the gain for specific frequencies of the audio signal. Operation of the equalizer is left to the end user. In a parametric equalizer, the audio frequencies of the audio signal are divided into bands, and the center frequency of each band can be fine tuned by changing the parameter Q (quality factor). The primary reason for providing this functionality in the R2J15116FP is to enable fine-grained adjustment of the speakers’ frequency characteristics.

* Product names, company names, or brands mentioned are the property of their respective owners.