11th November, Electronica, Munich - Renesas Technology Europe today
announced an expansion of its popular M16C Platform microcontroller*1 lineup
with 16 low voltage models that can operate down to 1.8V. These devices,
especially trimmed versions of the M16C/60 group, are fully compatible with
previous products.
The M16C/63 family of devices can operate between 1.8 to 5.5 V and utilise
the high-performance, M16C/60 16-bit CISC CPU core. At 1.8 to 2.7 V the CPU is
running at speeds up to 5 MHz. From 2.7 to 5.5 V, 20MHz operation can be
achieved.
In addition to the low voltage operation, the devices power consumption is
extremely low. In full active mode, with Vcc=3V, WDT, RTC and external 32kHz
crystal running and the CPU clocked at 20MHz, a total power consumption of 9mA
is possible. In the devices wait mode, with WDT, RTC and external 32kHz crystal
running, 3.5μA is achievable at Vcc=1.8V.
New features include a CEC (Consumer Electronics Control) circuit, a
low-voltage detection (LVD) circuit, real-time clock with full calendar
functionality (RTC), high-precision (40MHz) on-chip oscillator and a watchdog
timer with an independent oscillator (125kHz). A hardware multi-master I2C-bus
has also been added in place of the simplified I²C-bus.
The on-chip peripheral functions have been improved to include a fast A/D
converter, 6 USART, 2 SIO, CRC unit and 4 DMA controllers. The 10-bit A/D
converter achieves a fast conversion speed of 2.15 μs and offers 26 channels.
The devices are available with on-chip Flash and RAM memory in density
combinations of 128kB/12kB and 256kB/20kB. The ICs also have an extra flash
memory for data storage. Two banks of 4kB DataFlash*2 each, with an endurance
of 10,000 cycles in both read and write operations, as well as a bank of 16kB
to store a customised boot-loader are included. The M16C/63 will be available
in 80-pin and 100-pin QFP packages.
“With the 1.8 V operation of the M16C/63 we can now support customers to use
a limited supply voltage in their systems more effectively”, said Bernd
Westhoff, product marketing manager Reneas’ consumer, industrial and
distribution business unit, “With the pin-to-pin compatibility to other M16C
products, along with the attractive price and low current consumption footprint
making M16C/63 an easy choice for engineers. Further developments of the
M16C/63 product line-up will extend to even larger embedded memory of up to
512kB Flash.”
In addition to traditional industrial and consumer applications, the new
M16C/63 is particularly well suited for portable applications such as glucose
meters and metering application where low power consumption is important.
Furthermore due to the integrated CEC circuit, M16C/63 is an ideal solution for
a general power management unit in the HDMI environment for home entertainment
equipment.
The new E8a on-chip debugging emulator is available as a development
environment. The E8a can also be used as a flash programmer.
The M16C/63 group is currently sampled to lead customers and samples will
soon be generally available.
Notes to editors
1. M16C Platform family are CISC microcontrollers, comprising a varied
product lineup of 16-bit and 32-bit products in the M16C Series, M32C Series
and R32C Series. Features include highly efficient C-language support,
excellent noise characteristics, low power consumption, and comprehensive
on-chip peripheral functions. The range of low-end to high-end series featuring
the same architecture, pin assignment compatibility, and peripheral function
upward-compatibility provides support for a wide range of application areas,
including the automotive, industrial, and consumer fields.
2. DataFlash is Renesas’ own flash memory for data storage.