Home / Products / Software and Tools /

Flash and PROM Programming 


 
Provide feedback
Print this page



Flash and PROM Programming
Partner Information
Programming Methods
Programming Tools


Application Notes


Discontinued Info


Documentation


Downloads


FAQs


Technical Update



 



The Flash Development Toolkit (FDT) application is the latest FLASH programming interface supplied by Renesas. This can be used to support BOOT and USER mode flash programming for both Renesas devices in Development Kits and User's hardware. FDT supports many Renesas FLASH microcontrollers, with support for new devices added as they become available.

FDT is a 32-bit application that provides a workspace based environment. The user can create multiple projects where the target device and mode of connection can be selected, along with any specific communications requirements within a workspace. This allows for many forms of connection to Flash devices to be supported from a single workspace. The workspace also allows a number of data files to be included which can be merged to form a single 'image' file. There is a setup wizard to help create new workspaces customised to the user's requirements. The FDT Project Wizard will guide you through the necessary steps to create a project. The project wizard gives interactive help as you change settings. Simple Interface Mode and FDT Basic Mode allow programming using a simplified GUI.




Lineup:


Flash Development Toolkit Version 3.05


Renesas Flash Development Toolkit (FDT) Version 3.05 Release 00